This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256301 LLC部分可不可以使用低压调试(HVDC不使用390V,先使用50V左右调试)

Other Parts Discussed in Thread: UCC256301

^^

UCC256301 LLC控制芯片, 调试的时候能不能使用低一些的直流调试,例如50VDC或者100VDC,而不是直接使用390VDC

谢谢!

  • Hi
    不行的,在设计时,规格上总有个最低输入电压,你可以在这个电压下先测试看看,但是不会低到50V.
    如果担心烧板子可以在电源供应器上设置保护,或者增加测试板(在输入,我以前公司就是增加灯的方式做到,万一MOS烧掉,可以保护一下)