This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6508641其中BUCK5 1.2V输出过冲



目前在测试PI的时候发现,TPS6508641的BUCK5_1.2V在上电后一段时间后会出现一段过压尖峰(最高1.8V)。

于是做试验,断开BUCK5的所有负载,发现过压尖峰依然存在。然后查找其他地方有没有相关电压波动,也没有。其他各路电压也都正常。

然后找其他的板子测试,发现每块板子情况有些不同,有些尖峰比较厉害,有些由只是在1.1-1.4V震荡短时间后就没了。

然后去翻看TPS6508641的手册,发现这个芯片的初始非OTP版本TPS6508640的BUCK默认是设置在1.8V的。

有没有可能内部程序异常导致这个问题?是不是一个芯片的BUG?目前来看,我们并没有很好的手段从外部来处理这个问题。