This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC34063ADR芯片工作状态异常的问题



MC34063ADR,按照数据手册参考电路设计测试条件的条件下:输入电压24V、输出12V、负载功耗3.7W。进行测试,输入电流上电瞬间涨到0.177mA,随后涨到0.285mA。输出电压12.3V,加上负载掉到5.6V,逐渐增加负载当输出电流达到200mA时,芯片工作异常,输出电压变低。输出电流上电瞬间0.281mA,随着电压降低电流降到144mA。目前的状态就是芯片输出电流达200mA后芯片工作状态不正常,输出功率不足,与芯片手册所标注的最高1.5A输出不符。用同款ON或HTC则不会出现任何问题,不知道是什么原因导致TI芯片出现如此问题。

  • Hi
    1. 确认功率电感饱和电流是否足够? 对于降压,功率电感饱和电流建议为最大输出电流的1.3倍以上。
    2. 示波器确认电流保护是否因为noise 提前保护?
    3. layout上注意功率回路尽量小。