This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1 SOH更新跳变问题



目前我们使用BQ27542-G1时作为5000mAh的软包电池FG,最大充电电流0.7C。我们打算把SOH Percentage作为健康度指示显示在上层界面。但每一次充放电后SOH的值都会产生较大幅度的变化。

我们期望客户看到的健康度是从第一次充放电,100%开始随着充电次数的增加逐渐下降。但是不要出现连续两次充放电之间电池的SOH出现大幅度跳变。

有如下几个问题想请教:

1、请问是否可以将SOH值作为健康度参数直接进行调用呢,在BQ27542中如果我们想进行电池健康度的判断通常还有哪些方法。

2、观察手册中看到这个SOH值与QMAX、RMC以及FCC有关,请问是否可以固定其中的值达到相似的目的。

3、我们发现每一次充电FCC都会和RMC产生较大的变化。是否有办法避免这样的现象产生。

4、在实际中发现标称容量会将开机电压之前的电量以及SOC满电电量之后的涓流部分统计的电量刨去导致标称容量每次计算差别很大。请问是否可以固定标称容量以便显示给用户增加体验。