This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps61088如何进行恒流

Other Parts Discussed in Thread: TPS61088

用一个21700电池做源(最大30a输出,2.8~4.2v),现在我想设计一款输出6v 3a 的可换挡的可调电源,请问有方案吗?

控制LED的 ,尾部按键,利用关断实现100 50 25 三种亮度 ,也就是说输出3a 1.5a 0.75a 三种恒流。谢谢。

目前打算用61088实现这个功能,但是后续的恒流源我无从下手了,最好有现成的参考设计,非常感谢

  • Hi
    区别于一般的恒压设计采用分压电阻将反馈信号给到FB脚,恒流设计是采用sense电阻侦测负载电流,将反馈信号给到FB脚。反馈信号可以通过运放进行高边采样,也可以直接将sense电阻电压信号直接给到FB脚,但是TPS61088 反馈基准是1.2V,直接反馈会造成高损耗,建议增加运放。