This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2013充电问题



请教一下,我的电池计量芯片用的是BQ2013、电池容量4800mah,使用情况如下:

1、经过一次老化(充满一次、完全放电一次)。由于完全放完电时,VDQ标志==1,然后再充电LMD寄存器被更新为:150;

2、老化后的第一次充电,直到NAC为LMD时,NAC不再增加。此时我认为:老化后的第一次充满电完成;

3、接着我做放电实验,当NAC为0且等到VDQ==1时,我再充电,LMD被更新为:115,LMD小了很多;

 

根据RS电阻计算,LMD==150是正确的,

问题:老化后,电池的正确充电应该是怎样的,是NAC==LMD就算是充满或者是别的什么情况?怎么样操作才是一个正确的流程?