This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ7790511电流采样脚短路



工程师,您好:

              现将IC(BQ7790511)应用于10串7并项目上,一级放电保护电流为40A(RSNS=1.25mΩ),经充放电测试、OCD1及SCD测试后,20个产品中有7个MOS管损坏且铜皮烧毁,经测试后发现IC(BQ7790511)的SRP与SRN短路(阻值约2Ω),IC检测不到电流也就不会进行保护动作。

              请问这种SRP与SRN短路的失效模式,常见的可能的原因有哪些,谢谢!

祝生活愉快!