This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3525AM: 对于Buck控制芯器的一点问题

Part Number: UC3525AM
Other Parts Discussed in Thread: LM5146, LM5143-Q1

想咨询一个问题

1. 想设计一款48V转28V的Buck,50A输出,能否用3525做控制器,或者有什么其他的推荐控制器

2.对于一个控制器而言,他的作用在于闭环控制,那么为什么会对输出电流也有限制呢,比如LM5146输出电流限制20A  

如果我的MOS管电流应力足够,不是可以输出超过20A吗,是不是这里是5146自身驱动能力有限,只能驱动这么大的电流 这个20A是怎么计算的

3. 如果我想输出更大的电流,是否把5146驱动接到一个驱动能力更强的驱动器,然后再接MOS管即可

还望大佬不吝赐教

  • Hi

       类似LM5146,  首先是受限驱动能力,其次做这么大功率,选择的MOS, 电感都有难度,是可以并联,但是并联也会有问题,例如layout影响等。选择电感,可能会有发烫的问题等等之类。一般DC/DC电流大了,都是采用2路甚至多路并联输出的方案, 类似LM5143-Q1.

  • 1.那请问这个驱动器需要sink或者source多大电流怎么计算呢,有TI技术文档可以参考吗

    2.之前用SG3525加推挽设计过大功率的Buck,想问下大功率Buck的布局有没有TI技术文档可以学习一下的

  • Hi

        没有计算文档,一般都是建议先择尽量小Qg的MOS.

        关于layout,一般都是对应芯片datasheet里面会详细提及,特别是buck芯片,但是没有专门的文档来说明。特别是类似SG3525这类PWM隔离方案芯片。