This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28084: 请教TI工程师UCC28084的CTRL引脚控制电压的设计

Part Number: UCC28084


TI工程师您好,最近在用UCC28084设计一款DC 12V~20V输入,DC 20V 2.5A输出的开关电源,开环控制。想用输入电压来控制CTRL引脚,从而根据输入电压的变化来相对的控制输出电压的稳定。

根据TI文档slua584a进行了电流检测电阻和补偿电阻的计算:电流采样电阻RISENSE经计算采用阻值为45mΩ的合金电阻,CS引脚上的电阻RF采用1kΩ电阻,设置ISLOP补偿电流的电阻RSET经计算为15.67kΩ,采用16kΩ的电阻。

我现在的疑问是电流型拓扑是控制电流峰值的稳定,即用CTRL引脚上的电压与CS引脚上的电压进行比较控制输出PWM的占空比。那么输出电压与CTRL输入电压以及CS引脚上的电压的关系式是什么呢?也就说我改如何设计计算CTRL引脚的外围电路参数呢?