This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117: CC/CV 设计如何提高输出电流/如何调K值问题

Part Number: LM5117
Other Parts Discussed in Thread: UCC28950

亲爱的TI技术支持:

我现在在用LM5117设计一个设计一个15V55V输入,12v,44A输出的CC/CV变换器。先提如下问题:

为了深入了解使用LM5117设计buck电路,我使用TI参考文章《How to Design a Simple Constant Current/Constant Voltage Buck Converter》(参考原理图如下,但调试时使用其它电源模组供10V电压)调试了一个CC/CV变换器,通过先调CC,再调CV的方式调出了一个有稳定输出的波形的东东,但存在以下问题

问题A: 设计为6A输出,但只能输出5A

问题B: 调出的K值不是1: 最后调出的参数: L0=33uH, Rs=0.04  Rramp=127k, Cramp=1000 pF. 就是说,在Rramp, Cramp, RSL0之间选择时调到了稳定工作状态, 但K值不是1, 有很大偏差,K值变成了差不多是6

问题C: 下行靠近最低工作电压(30V)时不能稳定工作。 

想搞清楚:在此情况下如何提高电流?