This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54260: TPS54260有关咨询

Part Number: TPS54260

        针对TPS54260的使用,有如下疑惑,请帮忙解答一下,谢谢!

1、我们的设计中电源唤醒和休眠的电压并不是按照同一个EN电压来判断,比如从低到高输入电压时唤醒为1.36V,从电压高到低进入休眠为1.1V。

2、当输入电压和输出电压的关系比如输出7V电压,那么最低的满载输出电压需要满足什么关系?VIN—VOUT大于多少 V?

  • Hi

        是的,1.36V以上才能保证启动,1.15V一下芯片关闭。

        这款芯片直接设计无法达到100%duty, 所以难以估算7V时最大输出电压,但是5V输出是没有问题的(主要还有就是最大duty也没有给出规格)