Part Number: TPS54620
比如tps54620降压芯片,我想要输入17V,输出13v,6A。用webench设计,此时效率96%,输入电流平均值为4.83A。而根据数据手册中“输入电容器的选择”相关章节,可计算输入纹波电流约为2.545A。那么是不是意味着我的供电电源必须满足17V,驱动电流至少要4.83A+2.545A/2=6.10A?还是说只要满足4.83A输入电流平均值的供电电源即可?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
无需到6.1A, 不需要按照峰值电流,按照均方根或者平均电流即可,建议保证5A(略大即可), 但是如果是升压芯片,就需要注意,那么就需要按照你现在的计算方式,采用平均输入电流加上电感纹波电流/2.