Other Parts Discussed in Thread: BQ25713,
输入是4节锂电池,计划放电电压范围是13V~16.8V,输出是12V5A,用网页模拟的原理图如下,实际基本按这个参数设计的,如下,现在测试,输入要达到14.76V的情况下,输出才能到达12.05V,而且电感还有声响,问一下这个芯片能不能做到13V输入12输出,可以的话参数应该怎么调整?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
能否将输入电压波形传上来看一下,建议输入电容适当加大一些(可以增加一个100uF电容,layout上尽量靠近MOS 输入处。
Hi
如果输入是稳定的,你可以按照datasheet 14页8.36 Dropout Voltage Reduction 来改善,通过调频率的方式就可以。
用示波器抓了,BQ25713的输出很稳定,刚才试了一下,只有在接近空载的时候才会出现这种输出不稳,然后电感有达达响的情况。然后接上300ma负载的瞬间有时候会有啸叫,之后输出就能稳定在12V左右了,电感的声音也消失了
Hi
加大输入电容, 和降低Dropout Voltage 能改善吗?
加电容改善不大,带载实测压降是不大的,比规格书里面的计算值还小一些
Hi
所以现在的问题是Dropout Voltage 改善了没有效果。那么就要确认duty控制了, 14.76V时duty到达多少?
再确认一下boot电容。