Part Number: UCC2897A
Other Parts Discussed in Thread: LM5026
您好,目前我设计一款DC-DC电源,输入66-160V,输出24V,200W,使用该芯片时,发现在输入110V时短路保护为打嗝模式,在输入70V时短路保护为恒功率模式(不打嗝),并且输入功率较大,电源发热严重,通过调节CS脚参数,均无法实现打嗝模式(我的电路芯片为辅助电源供电,短路时VCC电压不能降下去,持续供电)。从UCC2897A的资料文档中,没有提及过流及短路模式,从测试结果看,过流为恒功率模式,只有资料中的Figure 12提到CS脚电压在0.75V时为Hiccup Mode,请问如果实现打嗝模式,降低输出短路保护时输入功率,是否需要外加电路?能否实现LM5026芯片一样的短路模式?谢谢!