Part Number: LM76005
Hi
- 輸入電壓範圍至少達40V
- 輸出電流至少3.5A
- 工作溫度範圍寬溫(工規)
- 輕載高效率,輸入36V;輸出5V電流10mA效率85%左右
- 可調式或固定5V輸出都可以
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM76005
Hi
Hi
在内置MOS下的降压芯片list下设置一下条件,如输入电压>37V(留至少1V的buffer), 输出电流>3.5V, 特性中选择“轻载效率” , 就可以筛选出合适的芯片,你可以加更多条件,例如同步,价格等等再缩小范围:
但是按照你的条件选择估计很是很难找到,我查了很多个,都难以实现輸入36V;輸出5V電流10mA效率85%左右。一般降压芯片高压差难以实现高效率,如果你是12V输入,符合的应该不少,但是36V造成的高压差效率就会压低很多。