This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: LM5175和LM5176的区别是什么?

Part Number: LM5175
Other Parts Discussed in Thread: LM5176

TI工程师你好!

目前LM5176供货困难,是否可以用LM5175代替原有电路设计中的LM5176。这二者有什么本质区别?原有设计是输入8~36V输出12V /6A 。我使用WEBENCH® Designer 设计,LM5176可以满足这个需求,但是 LM5175只能满足输入8~36V输出12V/3A,超过3A就会提示(

Design cannot be created!

Your preferred device does not work with the inputs you selected.

OpVal table param temperature > 150°C

Please change your inputs or select another device.

是否5175无法满足我的设计要求呢?

  • Hi

        主要是输入电压范围,和导通模式上的差异, 见datasheet 第一页。

        其次2个芯片在参数上差异也很大,具体看2个芯片的参数表。

        但是2个芯片的功能上非常接近。

        

  • 请问下工程师,板子设计的是LM5175,是否可以不改设计直接贴片LM5176,是否是PIN-TO-PIN兼容,只是输入电压范围,工作模式,输出能力等有区别,但在一定范围内是通用的?

    期待您的回复。

  • HI

        功能上可以,但是不同芯片,从datasheet看差异还是很大的,不能兼容,换芯片要重新设计。

x 出现错误。请重试或与管理员联系。