Part Number: TIDA-01352
Other Parts Discussed in Thread: LM5030

您好,我正在使用贵公司的TIDA-01352的设计。测试时发现负高压部分没有输出,LM5030没有输出,且其VCC引脚处的电压只有3.8V,D6两端电压为3.8V。现在我怀疑是Q7的MOS管坏了,但这款器件不容易焊接。现在我想通过VIN引脚给LM5030供电,也就是焊上R45与C47,并且去除Q7,请问这样的方案可行吗?或者您有什么推荐的方案,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01352
Other Parts Discussed in Thread: LM5030

您好,我正在使用贵公司的TIDA-01352的设计。测试时发现负高压部分没有输出,LM5030没有输出,且其VCC引脚处的电压只有3.8V,D6两端电压为3.8V。现在我怀疑是Q7的MOS管坏了,但这款器件不容易焊接。现在我想通过VIN引脚给LM5030供电,也就是焊上R45与C47,并且去除Q7,请问这样的方案可行吗?或者您有什么推荐的方案,谢谢。
HI
我觉得很可能是D6损坏了,因为这个稳压管电压已经完全偏低了,建议先换换看。
当然你可以将这部分电路拿掉,直接外观供电Vcc来让芯片工作看看? 不能通过直接通过Vin来给,这里就是做一个regulation给芯片供电。
感谢您的建议,经过测试D6没有坏,直接外接供电后系统正常工作了,确认是Q7的问题。非常感谢!