This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24105充3S CoLiO2电池FB端电阻设置问题

Other Parts Discussed in Thread: BQ24105

应用手册上没找到怎么计算FB端电阻的,请问充3串电池的话FB端的两个反馈电阻设多少合适?

  • 计算的BQ24105的FB端反馈电阻的公式见datasheet的 page 15(Battery Voltage Regulation)

     Voreg=Vibat*(R1+R2)/R2,

     这里R1指靠近output端的电阻,R2指接地的电阻,而VIBAT是用于内部误差放大器的基准源,为常量2.1V, VOREG为期望的CV模式时的输出电压。

     通过这个公式可以观察到r1和r2的比率决定了CV模式下的输出电压,我们可以选择一个满足偏置电流要求的R2,比如100K欧姆 ,然后查阅你的COLIO2的规格书,找到单节电池充电时的指定CV电压,乘以串联的节数3,即得到需要的VOREG=3*Vcell,因此公式中只有R1一个未知量可以求出,根据计算的结果选择就近的实际电阻即可。注意反馈电阻要选择高精度(如1%),低温漂的电阻类型。

  • 非常感谢杨工的回答,谢谢!