比如说我需要始终维持3.3V电压给系统供电,电池电压是从3.7V开始往下降的,使用TPS61021输出3.3V可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
3.7V电池实际工作电压范围打算是多少? 2.5~5.2V, 甚至更低?
TPS61021是升压芯片,低于3.3V可以正常升压到3.3V, 但是高于3.3V输入没有问题,但是此时芯片工作在Pass-Through Operation模式下,并不能保证输出仍是3.3V, 而是输入电压减去电感DCR压降以及高边PMOS的压降。
建议你选择升降压芯片来做。
关于Pass-Through Operation, 具体见datasheet 第9页7.3.5。