This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B85-Q1: 输入电压和输出电压的关系以及UVLO检测输入电压的问题

Part Number: TPS7B85-Q1

Hi

请教下Spec中说,TPS7B85的输入电压范围是3-40V,输出是固定3.3V或5V。请问如果输入3V或小于3.3V时,输出会是怎样的?另外,关于7B85中的UVLO检测,具体是多少值?即UVLO检测输入电压阈值低于多少时,芯片不工作,输入电压达到多少时芯片开始工作?谢谢!

  • Hi

       首先作为LDO, 输入必须大于输出加上Vdrop,  也就是说你要输出3.3V或5V, 输入必须大于3.3V+Vdropmax或5V+Vdropmax。 而如果输入3V或小于3.3V时,此时的输出电压只能设置到3V-Vdropmax或3.3V-Vdropmax一下。

       欠压保护看datasheet第五页规格表, 如果Vin上升时,需要必须大于2.82V才能绝对保证芯片正常工作。

  • Hi Tao

    了解,那请问下表格8.1是什么含义?Input voltage指的是Vin还是Vsense_in?比如我R1设置18.2,R2设置10,怎么理解input voltage 3.3V, threshold voltage为3.13V?这个的VSI(low)是多少?是固定值1.12V吗?VSI(HIGH)是固定为1.21V吗?不太理解这一块,麻烦说明下这个UVLO机制,多谢!

  • Hi

       另一个帖子中已经回复。