Part Number: TPS7B85-Q1
Hi
请教TPS7B85的两个问题:
1. datasheet中8.1.6的表格是什么意思,比如Vsi输入为3.3V,如何通过R1=18.2,R2=10得到threshold voltage为3.13?
2. Vsi(high)的值是多少?在datasheet中没有找到
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS7B85-Q1
Hi
请教TPS7B85的两个问题:
1. datasheet中8.1.6的表格是什么意思,比如Vsi输入为3.3V,如何通过R1=18.2,R2=10得到threshold voltage为3.13?
2. Vsi(high)的值是多少?在datasheet中没有找到
Hi
Vsi输入为3.3V,如何通过R1=18.2,R2=10得到threshold voltage为3.13?, 这个不是通过算的,注意5% THRESHOLD, 我觉得是通过这个5%来算的。
Vsi(high)的值在参数表,见datasheet 第6页Sense input threshold high 1.17V 1.21V 1.25V
但是Vsi(low)的值参数表里也有,这里的3.13V是什么呢?按照我的理解,这个Vsi(low)应该是跟Vsi input有关吧,比如输入3.3V,再根据要求的精度如5%,得到3.13V,那参数表里的Vsi(low)是固定典型值1.12V,这个怎么理解呢?