This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9244: FUsion design电源管理

Part Number: UCD9244

您好

       使用UCD9244芯片去控制一路3.3V的电源输出,出现以下问题;

1.从Fusion Design上看到本应输出3.3V的电压为1.56V,检测到FLT的错误,具体指哪方面的错误呢。

2.从示波器测量的结果来看,输出的电压是0V(应该是电源芯片被UCD9244给关了,为什么和Fusion Design软件上的测试结果不一致)