This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3150 :Cbst value

Part Number: LM3150

Dear Sir.
LM3150 datasheet says Cbst is a 0.33 to 0.47-µF.
But the I wants to know what the Min. value of Cbst is.
What could happen if Cbst was set to 47nF?
And the SF is twice higher than the set value, Could you tell me why?
Your reply would be appreciated.
Design
Input Voltage : 14 ~ 24 V
Output Voltage : 8 V
Output Current : 5 A
Max Temperature : 85 deg
Switching Frequency : 130 KHz
Best Regard