This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: 器件上电容易损坏

Part Number: BQ76952


我在使用BQ76952芯片的时候,电池输入接口使用14芯LEMO插头,当和12S锂电池对接时,很容易就导致芯片损坏,结果就是I2C不能正常通信。但是当我使用稳压源进行模拟输入时,器件工作正常,不会出问题。我不清楚是因为什么导致芯片损坏,是上电时候的冲击吗?这个芯片耐压值为80V,而我的电源满电时,电压只有50.4V。我想请您这边帮忙分析一下故障可能的原因。

  • 您好,由于问题比较复杂,我需要询问更了解这款芯片的TI工程师,再帮您解答,稍后回复

  • 您好,The BQ76952 is generally very tolerant of random connection from a connector.  The cell inputs other than VC0 have 85V abs max limit.  VC0 has a low abs max limit and is recommended that its filter connect to the battery- and VSS on the PCB.  See section 16.3 Random Cell Connection Support of the data sheet.  Use the information and the customer connection diagram to evaluate any risk.