5V电路中,FB电阻选值计算电压是对的,R1=56K,R2=10K,拆下来量也是对应阻值,但是在PCBA上量R1=15K,R2=9.5K,按这两个值计算Vou是2V,实际Vout=9.5V。另一路3.3V设计中,R1是33K,R2是10K,实际Vout也是9.5V,请问各路大神这个可能会是什么原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
严重偏高,很可能是芯片FB脚损坏,换个芯片看看。
或者将FB电阻拆掉,测试FB脚阻抗,正常无穷大。