buck或buck-boos架构,
Vin 2.7-4.2V(电压在这个区间即可),
输出6V 5W.
恒流的1%调光比,
请帮忙推荐相关的型号。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
buck或buck-boos架构,
Vin 2.7-4.2V(电压在这个区间即可),
输出6V 5W.
恒流的1%调光比,
请帮忙推荐相关的型号。
Hi
推荐TPS61500, 不过这个芯片最低输入电压是2.9V, 欠压保护是2.7V以下,适合电池供电。
Hi
这个芯片推荐PWM调光频率推荐200Hz~1000Hz, 满足你的要求。
Johnsin:
如果是用模拟调光,可以达到1%的精度嘛?