Other Parts Discussed in Thread: LM5157-Q1
单节18650电池, 电压: 3.0~4.2V, 电流: 6A ;
驱动:5*5=25LED灯组,5串,5并。 所需驱动条件: 30V , 500mA
请帮忙推荐合适我电源IC方案。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
好像没有合适的方案,按照你的要求,输入3V时,15W输出,输入电流都超过6A. 只能选择外置MOS的LED 驱动,但是这类芯片输入电压一般都是高于3V的。
或者你可以选择LM5157-Q1这样的升压芯片来做,只不过需要额外用运放来做恒流设定。