This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请帮推荐,单节18650电池驱动15W LED灯组方案

Other Parts Discussed in Thread: LM5157-Q1

单节18650电池, 电压: 3.0~4.2V, 电流: 6A ;

驱动:5*5=25LED灯组,5串,5并。 所需驱动条件: 30V , 500mA 

请帮忙推荐合适我电源IC方案。

  • Hi

        好像没有合适的方案,按照你的要求,输入3V时,15W输出,输入电流都超过6A.  只能选择外置MOS的LED 驱动,但是这类芯片输入电压一般都是高于3V的。

        或者你可以选择LM5157-Q1这样的升压芯片来做,只不过需要额外用运放来做恒流设定。

  • 你好, Johnisin 

    使用外置mos的LED驱动,输放电压高于3V。  

    如果这样,用两路电压输入,1路高到3V(比如6V, 电池通过小的升压电路可以得到) 但是功率比较低 提供给芯片工作;

    另1路从电池引过来 给外置MOS升压,这种方式可以吗? 

    谢谢! 

  • Hi

        如果最终电源来自电池,例如2路级联,我觉得还是不行,因为低电压下峰值电流肯定超过6A.