This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD3138HSFBEVM-029: 在导入一个从贵司网站下载的工程后,编译一直无法通过

Part Number: UCD3138HSFBEVM-029

在导入一个从贵司网站下载的UCD3138HSFBEVM-029工程后,编译一直无法通过。 

一直提示有两个error : 

Error1: Program "make" not found in PATH

 ERROR2: This project was created using a version of compiler that is not currently installed - 5.2.4 [Arm]. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="">software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'. UCD3138HSFBEVM_029 properties Problem

我们已经被此问题困扰多日了,且试了多种方法也无法解决。

请知道的小伙伴们多多支持,不胜感激!

谢谢!