你好,
我们用的TPS566238,使用过程中发现,TPS566238及他的外围器件(主要是电感)在空载状态下,要消耗0.3W左右的能量,电感有小的啸叫,声音很轻,请问这是正常的么?请问一下TPS566238EVM的空载功耗大约是多少?我们的输入是13V 输出是6V,原理图如手册图,,C11焊接了,试了多个容值的电容(10p 68p 100p 200p以及不焊接),没有什么改变,我们的设计中没有R1这个0R的电阻。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
我们用的TPS566238,使用过程中发现,TPS566238及他的外围器件(主要是电感)在空载状态下,要消耗0.3W左右的能量,电感有小的啸叫,声音很轻,请问这是正常的么?请问一下TPS566238EVM的空载功耗大约是多少?我们的输入是13V 输出是6V,原理图如手册图,,C11焊接了,试了多个容值的电容(10p 68p 100p 200p以及不焊接),没有什么改变,我们的设计中没有R1这个0R的电阻。
Hi
空载时看输入电流,最大475uA, 如果乘以输入电压,大约6mW. 0.3明显异常了。
看一下输出电压这个时候是否严重震荡不稳定? 确认一下是否C5 Layout的影响。
你好。我们完全按开发板的布局做了改动,结果还是差不多。我用WEBENCH做设计的时候发现有个IC PD约240mW,请问这个是什么功耗。Total Pd约253.7mW,请问这个又是什么功耗呢?如图所示,
局部放大如图:
,这个是不是可以说,在我的负载很低的时候,这个电源系统的功耗就是这样的?这个数值和我们的实测值非常接近。我们静态时的输出电压用示波器看良好,虽然纹波没有手册上写的那样好,大约20mV的样子。