This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63070: 設定後端輸出5V,當負載小於1A時,後端電壓輸出正常。大於1A時,電壓會掉到3V左右。

Part Number: TPS63070
Other Parts Discussed in Thread: TPS55288

你好

最近在測產品,發現後端吃電約0.5A時,這顆的輸出電壓是在我的設定值範圍5.5V內

可是當吃電接近1.5A時,後端的電壓就整個掉下來在3V左右,而且還不穩定。

不穩定的原因,我推測是後端不是並不是穩定一直吃大於1A以上的電流,所以電壓又彈回又掉下來。

我用TI的WEBENCH來模擬,發現的確有這個狀況 (這邊也真的希望貴司工程師回覆前也能和我一樣先模擬) 。

並且,也在貴公司的國外設計論壇上看到有相關的回覆。WBDesign264_Startup-6.pdf

TPS63070: Can this device work in parallel configuration? - Power management forum - Power management - TI E2E support forums

  • Jasper Li  in reply to Yasushi Fujiwara
    TI__Mastermind 46095 points

    hi Fujiwara

    the TPS55288 is suitable for such high current application. TPS63070 doesn't work.

這顆晶片的DS寫的很清楚,支持到3.5A的輸出。

我的需求是5.5V 2A,請問是否適合,還是我要如何修改??

感謝。