This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD19536KTT: 大电流MOS管的散热问题与驱动问题

Part Number: CSD19536KTT
Other Parts Discussed in Thread: UCC23511-Q1

我想使用UCC23511-Q1 芯片驱动此款MOS管(272A),MOS管使用高端驱动,将要通过120A的电流,不知道这种驱动方式是否可以?而且我准备用两个MOS管(相当于分流保护)并联在一个驱动芯片上,不知道是否可以?

此MOS管最理想的电阻是2mR,经过120A的电流,功率有近30W,这是D2PAK封装的MOS管,请问如何散热?30W功率都快到电烙铁。还有一款MOS是2.7 mOhm的电阻 封装是TO220,热功率接近40W,请问哪种封装好散热? 

此电路不是PWM控制,而是控制电源输出,希望能在1ms内导通,导通后最多1S就会切断,几个小时内都不会再导通,请问这种上百A电流的电路板如何设计?如果只工作1s 还用设计风扇吗?

我只找到了最高100V的NMOS,请问如果需要更高的电压就不能使用NMOS了吗?

谢谢