想通过此芯片设计一款,输出可以调压的方式。因为输出电压有多个,进行公式计算也有多组值,不知道,如何选取电感,开关频率等参数。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
按照输出中心值计算电感,最大功率输出最小输入电压计算电感电流。频率是固定的,一般300kH~700kz,甚至更低一点。(频率高了功耗也相对高点)
反馈电阻按照输出中心值计算,然后可调信号通过电阻给到FB, 可调信号变化输出电压变化。
其次需要说明的是,一般输出可调建议用数字电源来做,因为可以动态补偿。而采用LM5122这类芯片,因为是固定补偿,所以只是在设定输出电压上下较小范围内补偿环路稳定,如果距离设计值较远,环路可能不稳定,造成纹波较大。不过你可以增加以及LC.