Part Number: TPS92641
VCC输出电压是否为固定8V,HG和LG脚电压可以到12V吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
内部LDO, 输出典型值8.5V左右。类似这样的控制芯片一般都是可以外部灌入电压到Vcc(即不用内部LDO), 所以你可以输入12V, 这样在高输入电压时是有降低芯片功耗的好处的,如果输入电压不高是没必要的。
同时8.5V并不低,驱动一般MOS都是没有问题的,并不一定要12V, 因为很多MOS Vth也就2~3V.