Part Number: TPS23881
基本情况:供电端使用TPS23881,受电端使用TPS2373-4。TPS23881全新未配置,使用官方电路制作PCB。在TPS23881的自主模式引脚配置7.7K电阻,使其工作在4线对90W模式下。
现象:上电后通过观察供电电源,电流微变,通过示波器观察,根据手册判断为正在识别,一直不能识别成功。将TPS7343模块接至POE供电交换机,TPS7343模块工作正常,排除TPS7343问题。随后在此模式下只接2线对,发现可工作在2线对30W模式。
问题:1.TPS23881如何确定4线对时使用的是哪两个通道组成的4线对?
2.TPS23881是否需要配置寄存器才能工作在4线对?