Part Number: TPS1663
我在使用TPS16630在低温-40℃测试,电路限流值5A,输入电源为28V,电子负载设置为恒功率60W,开启电子负载后过了几十秒芯片保护了,我想问下我设置限流值为5A为什么芯片保护了,我查看芯片工作温度为-40℃-85℃
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS1663
我在使用TPS16630在低温-40℃测试,电路限流值5A,输入电源为28V,电子负载设置为恒功率60W,开启电子负载后过了几十秒芯片保护了,我想问下我设置限流值为5A为什么芯片保护了,我查看芯片工作温度为-40℃-85℃
Hi
看一下常温下是否正常?
低温-40℃下在芯片允许的温度下,但是芯片周边的电容容值会下降,可能影响到芯片的工作,你可以比较常温,和低温下的波形,然后适当增加电容容值确保芯片正常工作。