Part Number: TPS54560B
Other Parts Discussed in Thread: LM4040, TPS54360
用TPS54560B作为一级电源,输入范围9~28V,输出5V(输出电流700mA左右),常温下,当输入电源由9V逐渐升到28V的过程中(手动调节直流稳压电源),TPS54560B芯片的输出电压由4.92V逐渐升高到5.02V(对应测试FB管脚的电压由0.784V逐渐升高到0.799V),有2%范围变化,这个电压变化会造成设备的测量精度变差,有没有办法提升TPS54560B芯片的输出精度,提升至0.2%左右?我目前的想法是可不可以利用基准电压源,比如LM4040,产生一个稳定的0.8V电压,接到FB引脚,如果FB引脚的电压稳定在0.2%的范围变化,就可以提升输出精度,不知道这个方案有无风险?或有没有更好的解决方案?