Part Number: LMG1210
When I send 50% duty cycle, 500KHz complementary pulse signal to the hi and Li of lmg1210, and add epc8010 chip to the back end, the continuous pulse waveform will be output and flicker. How to solve this problem
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMG1210
When I send 50% duty cycle, 500KHz complementary pulse signal to the hi and Li of lmg1210, and add epc8010 chip to the back end, the continuous pulse waveform will be output and flicker. How to solve this problem
HI
从电路上看你用了很多变阻器,你是要做测试电路吗?
驱动上的电阻不可以打的,10ohm一般就很大了。 电路建议你参照datasheet,或者一些评估版。
我把电阻调成10ohm以下了,斩波输出的波形还是时有时无,我是按照datasheet里面的案例电路搭建外围电路的,可结果还是一样。
HI
首先Vin电容layout尽量靠近Vin脚,测试BST电压正常, 接着使用的是肖特基二极管, 检查chargupump电容是否异常?
然后就是正常的PWM输入,这个是被动器件,不应该出现这样的输出驱动信号?
(使用的MOS Qg尽量选小一点)



当我后面不接EPC8010,测得的波形是这样的,这个看起来正常,可是一接入EPC8010就变得一闪一闪的