Other Parts Discussed in Thread: LM51561, LMR14030
输入电压为12V,输出电压为6V-3A,LMR14030-Q1为二级电源,输入电压由前级电源LM51561反激拓扑结构提供12V
输出电容打算用一个47uF,一个106,一个104.
我看图片有点模糊,我附了个文档
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输入电压为12V,输出电压为6V-3A,LMR14030-Q1为二级电源,输入电压由前级电源LM51561反激拓扑结构提供12V
输出电容打算用一个47uF,一个106,一个104.
我看图片有点模糊,我附了个文档
Hi
电路直接用TI在线仿真确认即可。
输出电容可以增加106电容降低ESR, 但总容值要足够。也可以增加0.1uF陶瓷电容消除spike。
需要注意的是layout需要参考datasheet,这个对电源很重要。
这个芯片比较简单,输出电容以及输出纹波再调整也可以。