This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5176: 在进行24V输入19V输出的负载测试时,出现负载达到19V 6A时,输出端无法保持稳定输出。

Part Number: LM5176


问题背景:用LM5176 (HTSSOP-28封装)制作的直流电源在进行输出为19V的负载测试时,当负载达到6A时出现了输出端无法保持稳定输出的情况,5A以内都还正常。

关键元件参数:NTMFS5C670NLT3G(N-MOS Vdss=60V Id=71A Vgs=±20V)、WHC1770 (一体成型功率电感10uH 15A)。

波形数据:SW1的波形存在占空比减小又回复的情况,GND平面存在Vp-p = 100mv的噪声,高侧栅极开关H1波形上升沿存在较大的扰动。