Other Parts Discussed in Thread: TPS23753, PMP8803
TI工程师你好!本人按照PMP8803原理图,做了输出12V的1A的电路,通电进行测试,在测试过程中,发现输出端未接负载,TPS23753出现无法被PSE识别。而TPS23753外接负载后,则可以正常检测,分级,输出供电,做了几块相同阻容值的PCB板子,一样的阻容值。只有一块板子可以在不接负载的情况,空载情况下,正常被PSE识别,有效的输出12V,而另外几块板子,则通不过PSE检测,而是反复出现检测,分级,短暂输出12V的电压,后断开,重新检测。。。。。而在检查电路过程中并未发现PCB板上器件异常的情况。但是,其余的板子一接上负载,立马可以被PSE识别,正常供电,请劳烦帮忙分析一下,在什么情况下,会出现TPS23753接上负载能并PSE识别,不接负载则不能被PSE识别,而进行供电。