This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27426EVM-738: 如何解决电池做Leraning cycle中的压降问题

Part Number: BQ27426EVM-738


我们使用BQ27GDK000ECM+BQ27426EVM-738做电池建模,充放电电流为2A;

在充电循环结束后,电池电压实际测量4.1V(电池满电应为4.2V);

在放电循环结束后,电池电压实际测量3.6V(建模设置截止电压为3.4V)

问题:

电池以2A充放电会有200mV的压降,这一部分需要在工具那个位置进行补偿?