This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78Z100: BQ78z100 IC的Hardware version问题

Part Number: BQ78Z100
Other Parts Discussed in Thread: BQSTUDIO

我们BQ78z100上上批进料的IC,用bqstudio下命令读取HW version,返回的值是0x0B;BQ78z100上批进料的IC,用bqstudio下命令读取HW version,返回的值是0x03,中间还混有一部分读出来是0xFF的;这批IC进料,用bqstudio下命令读取HW version,返回的值是0x02,中间也混有一部分读出来是0xFF的。我的问题是:1. 同一批IC中为什么会混有HW version为0xFF的?2.不同批IC的HW version不同,差异在哪里?哪个版本才是最新版? 

  • 您好

    为什么会混有HW version为0xFF,非常抱歉没有查到相关信息。

    硬件版本存储在硬件平台自带的内存中,这不是数据闪存或指令闪存的一部分,您可以通过下载最新版固件并运行固件,这已经意味着硬件和固件之间的匹配。

    网上现在最新版的固件是0.05

    That information is in the firmware install folder:

    ===================================
    bq78z100 v0.05 (build 6)
    ===================================

    Fix issues found:
    - Some units could drive the thermistor pin low on power-on

    ===================================
    bq78z100 v0.04 (build 5)
    ===================================

    Fix issues found:
    - The gauge could become unresponsive in HDQ mode

  • 谢谢您的解答,不过您答复的主要是firmware固件版本的差异在哪里,我们更想了解Hardware硬件版本的差异在哪里。目前我们用bqstudio下命令读取Firmware固件版本为0x04,这个应该是IC出厂的固件版本,固件版本相对来说比较固定,但是对应的Hardware硬件版本却有很多,比如前面提到的0x02,0x03,0x0B,0xFF等。对于固件版本为0x04的IC,打开bqstudio时不会自动进入,因为bqstudio无法自动识别0x04版的固件,不过可以手动用0x05版的固件程序打开,用0x05版程序设置参数后转srec文件,未来用bqstudio烧录新的IC时,固件版本也会变为0x05,硬件版本会变为0xA2或0xA3,这些我们都试过。但是我们厂内是用自动化设备烧录,自动化设备不会改动IC的固件和硬件版本,所以IC出厂的固件和硬件是什么版本,出给我们客户就是什么版本。现在不太能理解的是,为什么固件0x04对应的硬件版本很多?我们客户问我们不同硬件版本之间的差异,我们也无法解释。

  • 您好,关于硬件版本的信息看到您已经在E2E英文论坛发帖,请继续关注。

    e2e.ti.com/.../bq78z100-hardware-version-problem