常温工作情况下,示波器监测EN信号、12V供电和PWM信号都正常,输出LED+电压从28V直线下降到22V左右,然后缓慢下降到12V。此时FB管脚电压1.4V左右,使用万用表测量FB管脚,故障会消失,输出电压恢复正常,FB管脚电压1.2V。故障反馈脚没有拉低。
故障出现后有时会自己恢复正常输出电压。有时会一直保持12V输出。
故障概率10%
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
常温工作情况下,示波器监测EN信号、12V供电和PWM信号都正常,输出LED+电压从28V直线下降到22V左右,然后缓慢下降到12V。此时FB管脚电压1.4V左右,使用万用表测量FB管脚,故障会消失,输出电压恢复正常,FB管脚电压1.2V。故障反馈脚没有拉低。
故障出现后有时会自己恢复正常输出电压。有时会一直保持12V输出。
故障概率10%
Hi
很可能是虚焊,建议你用热风枪吹一下,看看效果?(以前遇到过应该是虚焊导致的)
Hi
芯片fb脚虚焊,或者如果连接LED是cable线的,有可能松动造成接触不良。这些甚至可能导致芯片损坏。