This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ30Z55 不带二次保护IC,FUSE通过100k电阻连接到GND,PTC通过10k连接到GND,触发FUSE和PF



BQ30Z55 不带二次保护IC,FUSE通过100k电阻连接到GND,PTC通过10k连接到GND,触发FUSE和PF。

BQ30Z55 does not have a secondary protection IC. FUSE is connected to GND through 100k, and PTC is connected to GND through 10k to trigger FUSE and PF.

1. 4-cell li-po,FUSE通过100k连接gnd',测量fuse引脚电压为8.7v,发0029也清除不掉错误,请问FUSE引脚在什么情况下会被触发输出高。

1. 4-cell li-po, FUSE is connected to gnd' through 100k, and the voltage of the fuse pin is measured to be 8.7v, and the error cannot be cleared by sending 0029. Under what circumstances will the FUSE pin be triggered and output high.

2. FUSE通过100k连接gnd,之前发送0029无效,0012复位也无效,电芯电压降到4v一下也无效,我怎么操作可以清除了FUSE和PF变为绿色,问题是FUSE有检测功能吗?

2. FUSE is connected to gnd through 100k, the previous sending of 0029 is invalid, 0012 reset is also invalid, the cell voltage drops to 4v, it is also invalid, how can I clear FUSE and PF to green, the question is, does FUSE have a detection function?