This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: DSG Additional Circuitry 相关问题咨询

Part Number: BQ76952


BQ76952应用中,Q4能否省去,省去的话会给电路带来什么问题吗?

  • 您好,不建议将Q4去掉。

    DSG does not go below VSS, so without the clamp circuit of Q4 the gate of Q3 would remain near 0V and Q3 would operate in a source follower mode while a reverse charger was attached.  With Q4 on Vgs of Q3 is about 0, Q3 remains off and PACK+ falls to a negative voltage.  This creates a large voltage across R39 and R41 which are sized to dissipate the power required in that condition.  Since R39 and R41 are a large value to keep the power dissipation manageable, turn off would be slow, so D10 and R40 operate in parallel for DSG turn off to turn off the Q3 in a suitable time. 

    See the application note https://www.ti.com/lit/pdf/sluaa09 section 2 for test result and additional description.