This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: 电池管理芯片BQ4050的LED显示问题

Part Number: BQ4050


BQ4050能否支持4个LED显示电量,显示的电量分别为1个LED为25%,2个LED为50%,3个LED为75%,4个LED为100%。还是只能5个LED显示电量,1个LED为20%,2个LED为40%,3个LED为60%,4个LED为80%,5个100%。

如果支持4个LED电量显示,有没有软件配置用例。