datasheet中8.2.2 Figure39电路图中几个元器件的作用没太理解。
1.这个电路的目的是反极性,反极性的意思是VOUT和GND接反了?还是VOUT接到了比VIN还要高的电压?还是都包括?
2.D5是如何起到在关断时候,能够快速关闭MOS管的?除了这个方式,还有其他方式可以快速关闭MOS管吗?
3.D6,Q3,R2说是在反向时防止Q2,VGS电压过高被击穿,他看他的原理是当GND接高时,Q3导通,Q2的GS电压就是三极管Q3的压降了,这样限制了GS电压,从而保护。如果我说的正确的话,D6是什么作用?
4.是接着第三个问题说的,如果我的第三个问题描述的思路是正确的,把D6,Q3,R2删掉不可以吗?删掉后这部分电路后,Q2的VGS电压是怎么会变高的?还有我在Q2的VGS加稳压管能不能取代这个作用?
5.当VOUT和GND反接时,GND为高压,那不会从OVP,UVLO电阻倒灌到VIN吗?这样岂不是没有防反作用了?
6.D1的作用,只说了防止极性反转,怎们防止反转的没太明白,可以具体描述一下吗?