This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: 电源管理论坛

Part Number: UCC28780


您好:

           我是一名电力电子研究生,在调试UCC28780时启动过程出现了问题,希望可以得到各位大佬的帮助。

           在调试中,为了方便调试,我只焊接了UCC28780 周围的器件,在调试前,我已经认真阅读了UCC28780 的数据手册和调试手册,已经连接的电路如图1所示。8182.pdf

             根据调试手册调试流程,我首先将反馈脚FB经RFB接地,辅助绕组未接,SW脚接25V电压,得到的波形如图2所示,其中。紫色为VDD,黄色为HVG,绿色为REF参考电压。

可以看到VDD每隔一段时间会出现下降斜率增大的情况,而就是在这种情况下,才会触发大约2ms的RUN口输出,RUN脚间隔输出时间为1.4s左右,所以我猜测是触发了某种保护,但未调试成功,希望各位帮忙分析下。另外,在RUN脚输出后的2us后pwml 会输出5V脉冲,但只有一个,持续2us左右,如图3所示。

             因为调试手册说明只有出现4个pwm波才是正常的,但是按照调试手册的去检查发现也没有问题,希望各位大佬能帮忙解决下,如果也遇到这种问题,可以联系我,一起讨论下,谢谢大家