This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A8300: 想找一个输出电压可调范围6V-2V的LDO,请帮忙推荐一下型号

Part Number: TPS7A8300
Other Parts Discussed in Thread: TPS62170

想找一个输出电压可调范围6V-2V的LDO,请帮忙推荐一下型号

可以是一个LDO或者DCDC的电路,需要输出2V-6V左右的电压,电流大约300MA左右,需要可以通过程序控制来实现电压的调节。